Other Parts Discussed in Thread: TCAN4550
Dear Max Megee
I heard ceramic resonator of frequency accuracy is 0.3% can use a clock of IC with CAN-FD when operating at CAN-FD speeds from customer and standards organization.
If oscillator accuracy for CAN-FD is 0.15% when PLL uses, Is PLL frequency accuracy of 0.35%?
I think 0.15% is too tight.
Please tell me the reason that IC need oscillator accuracy 0.15% when CAN-FD use.
Could you share datasheet of TCAN4550?
Ishimasa