This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

DS90UB940-Q1: Is VGA @60 RGB565 possible with Internal TPG(Test Pattern Generator)?

Prodigy 220 points

Replies: 2

Views: 91

Part Number: DS90UB940-Q1

hello,

I want to know if  RGB565 VGA output is possible by embedded TPG as following settings.

        // disable tpg
	DS90UB940WriteReg(0x65, 0x00); //Internal clock enable for TPG

	//DS90UB940WriteReg(0x37, 0x12); // 2data lane, 1csi active.

	// set timing
	DS90UB940WriteReg(0x66, 0x00); //Red sub pixel
	DS90UB940WriteReg(0x67, 0x00); //Red sub pixel
	DS90UB940WriteReg(0x66, 0x01); //Green sub pixel
	DS90UB940WriteReg(0x67, 0x00); //Green sub pixel
	DS90UB940WriteReg(0x66, 0x02); //Blue sub pixel
	DS90UB940WriteReg(0x67, 0x00); //Blue sub pixel
	
	DS90UB940WriteReg(0x66, 0x03); //Clock Divder for VGA @ 60
	DS90UB940WriteReg(0x67, 0x08); // 

	
	// H & V total : refer to VESA VGA

	DS90UB940WriteReg(0x66, 0x04); // H total(800, 0x320) LSB
	DS90UB940WriteReg(0x67, 0x20); //

	DS90UB940WriteReg(0x66, 0x05); // V & H total MSB
	DS90UB940WriteReg(0x67, 0xD3); //

	DS90UB940WriteReg(0x66, 0x06); // V total(525, 0x20D) LSB
	DS90UB940WriteReg(0x67, 0x20); //

	// set H sync

	DS90UB940WriteReg(0x66, 0x0A);
	DS90UB940WriteReg(0x67, 96);

	// set V sync
	DS90UB940WriteReg(0x66, 0x0B);
	DS90UB940WriteReg(0x67, 2);

	// set Hbp
	DS90UB940WriteReg(0x66, 0x0C);
	DS90UB940WriteReg(0x67, 48);

	// set Vbp
	DS90UB940WriteReg(0x66, 0x0D);
	DS90UB940WriteReg(0x67, 33);

	// H & V activ
	DS90UB940WriteReg(0x66, 0x07); // H actvie(640, 0x280) LSB
	DS90UB940WriteReg(0x67, 0x80); //
	
	DS90UB940WriteReg(0x66, 0x08); // V active LSB & H actvie MSB
	DS90UB940WriteReg(0x67, 0x02); //
	
	DS90UB940WriteReg(0x66, 0x09); // V actvie(480, 0x1E0) MSB
	DS90UB940WriteReg(0x67, 0x1E); //

	// set H(-) & V(-) pol
	DS90UB940WriteReg(0x66, 0x0E);
	DS90UB940WriteReg(0x67, 0x03); 
	
	DS90UB940WriteReg(0x6A, 0x20); // forced to 2 lane

	//set output format RGB565, RGB444
	DS90UB940WriteReg(0x6B, 0x20); //CSI-2 data type 0x22

        // set tpg
	DS90UB940WriteReg(0x64, 0x11); // white raster pattern
	
	DS90UB940WriteReg(0x65, 0x04); // select Internal clock enable for TPG

Thanks.

  • Hello Kyoman,

    As explained in TI application note AN2198 (www.ti.com/.../snla132c.pdf) section 2.1, by default the pattern genrator operates in 24-bit color mode, where all 8 bits of the RGB sub-pixels are active. Only other option for use in patgen is 18-bit color mode (RGB666). This is selected in register 0x65 (Pattern Generator Configuration).

    Also, please refer section 3.2 of AN21989: Pattern Generator module is configured only with indirect address 0x00 to 0x17. You are using in above code CSI-2 data registers 0x6A, 0x6B. They are not applicable in internal patgen operation.

    By the way, fyi, you can also use ALP "Pattern Generator" tab and configure the settings to see Patgen operation.
    Thanks,
    Vishy
  • In reply to Vishy Viswanathan:

    Thank you.
    I understand.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.