Other Parts Discussed in Thread: TPS2514, TUSB422, , TPS65987D
Q1 I have a new dongle product which has one DC power source connector and a type-c connector . When there is no DC power source ,the the type-c of the product is in UFP mode and it can be charged by the type-C , 5V/1.5A is enough. When there is a DC power source ,the type-c of the produce is in DFP mode, the prodocut acts as a type-c powre charger ,the output is 5v/3a max .It can charge some mobile devices such as IPHONE, macbook .Do you have a good IC to be adviced.