Hello,
I have some questions for TUSB8041 configuration.
1.
Only one port(PORT1) is connected to external and power control is required for this port.
All other 3 ports(PORT2-4) are connected internally and power control is not required for them.
In this case, does the below configuration make sense?
FULLPWRMGMTz/SMBA1/SS_UP = 0
Unused OVERCUR2-4 = 10K ohm external pull-up
Unused PWRCTL2-4/BATEN2-4 = leave open
2.
If using a port for only USB2.0, is it OK to leave open for USB_SSTX and USB_SSRX pins?
3.
I want to use external clock source for input clock.
But the external clock is 3.3V signal. So I’m considering to use it with a resistor divider.
Does this way work? If it could work, how much ohms is good for this?
Regards,
Oba