This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB933-Q1: DS90UB933-Q1 and DS90UB954-Q1: Urgent .

Part Number: DS90UB933-Q1

Hi, I have sent an enquiry few days ago, but I did not get a reply yet.

My Questions:

I trying to connect this 933 in the following configuration:

1.  Mode setting : External oscillator  mode using 48 Mhz crystal

 2. Pclk is from  Image Sensor  is 96Mhz connected to PCLK of the  933

 3, My sensor feed in  to 933 is 8 bits instead of 10 Bits

       Din 0 to Din 7,of 933 inputs connected  to  Data0 to Data7 of my sensor  output

       Din 8 to Din 11 of 933 input is connected to Gnd.

Does this work for the 933?

Deser connected is  DS90UB954-Q1..Output form 954 is MIPI with a 25 Mhz Clock Crystal...Mode set to Raw10

Thank You