This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TUSB9261: TUSB9261 SPI flash

Prodigy 20 points

Replies: 4

Views: 110

Part Number: TUSB9261

Hi,

I have build up an USB-SATA Interface with SPI flash of Mircochip: SST25VF512A . It will be flashed by the TI Windows Flash Burner tool. But the firmware doesn't start. The TUSB9261 is still in bootloader mode. Does it depend on the internal unchangeable bootloader software inside the TUSB9261 or depends it on the Firmware 1.05 or 1.06?

Br

Bjoern

  • assign to Nick.
  • Hi Bjoern,

    Please confirm that the SST25VF512A is connected as shown in the TUSB9261 USB 3.0 to SATA Bridge datasheet in section 8.2.2.4 and that the SST25VF512A meets all the specifications described in that section.  Figure 3 shows a schematic of how it should be connected.

    The bootloader for the TUSB9261 is stored on ROM inside the TUSB9261; the firmware should be stored on the SST25VF512A.  Assuming you have followed the steps described in the TUSB926x Flash Burner User Guide and successfully loaded the firmware onto the SST25VF512A , the bootloader will retrieve the firmware from the SPI Flash on startup.

    Nicholaus Malone

    Applications Engineer

    High Speed Signal Conditioning

    Please click This Resolved My Issue if the reply answers your question.

  • In reply to Brian Zhou:

    Bjoern,

    Did this answer solve your problem? If so, please let me know and mark as resolved.

    Nicholaus Malone

    Applications Engineer

    High Speed Signal Conditioning

    Please click This Resolved My Issue if the reply answers your question.

  • In reply to Nicholaus_Malone:

    Marking as resolved due to inactivity.

    Nicholaus Malone

    Applications Engineer

    High Speed Signal Conditioning

    Please click This Resolved My Issue if the reply answers your question.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.