• TI Thinks Resolved

DS92LV010A: LVDS to TTL

Prodigy 50 points

Replies: 4

Views: 54

Part Number: DS92LV010A

Hi,

I need do translate LVDS to LVTTL/TTL logic level.

I only have 5V Vcc.

I fount the DS92LV010A (didn't find a single receiver - are they any?).

Is it safe to use it as a regular LVDS, with 100ohm input diff. termination, (and interface transmitter like the DS90LV011)?

 by datasheet, it designet do work as part of a bidirectional bus, with diff. 27ohm termination.

(I also found the DS90LV019, but it's a 16-pin package for a single receiver..)

Thanks!

Max