I have the 8881EEVM and am using it with the MC33033 TO CONTROL A 4-PHASE motor. Problem is the EEVM comes with R3, R4 Resistor banks which have to be disconnected. I don't have the skills or equip to do this, it is SMT Is there any solution i.e. can I get the EEVM without R3,R4 or can I get the DRV8881E on a board with pinout connectors?