Tool/software: TI-RTOS
I use UB925 and UB940 to form FPDLINK to output video signal.I am sure that the clock and sync signal are entering UB925.Some one asks me to detect lock pin of UB925.but I have not found this pin.
Since I don't have a schematic of the 940 part, the 940 clock and sync signal are not easy to detect.Is there any other way of testing?
UB940 has default settings
I config 925 like this:
0x01=0x02;
0x03=0xab;
0x04=0x8a;
0x12=0x8e;
I can get the address of 940 in the register 0x06 of 925.
Is that right?
thanks
chengbo