This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

SN65C3243: Data Rate Clarification

Prodigy 475 points

Replies: 1

Views: 56

Part Number: SN65C3243

The summary says operation from 250kbits to 1Mbit.  It then says the minimum "Maximum data rate" is 250kBits. Can you confirm that this part will work at all speeds slower than 250k bits using a 3.3V Vcc?

  • Genius 12395 points

    Matt,

    Yes, the device works with the signal whose data rate is slower than 250kbps with a 3.3V supply. Maximum data rate section on the datasheet shows the fastest data rate the device supports with different loading condition.

    Regards,

    Hao

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.