Hello,
I'm struggling to configure a DS90UB953 serializer with a DS90UB954 deserializer in RAW10 mode.
My input timing configuration is:
Pixel Clock: 88MHz
Active area: 1280x720
Horizontal blanking: 500
Vertical blakning: 100
CLOCKIN(reference clock) = 50MHz
The connection between the transceiver is coaxial mode(single ended, 50Ohm).
I would like to know exactly what register are need to be configured to have both the transmitter and the receiver succesfully comunicate in RAW10 mode (only one port, port 0).
Also an example with different timing would be helpful.
Thanks
Best Regards,
Fabio