Dear TI Experts,
Can I use DS90UB913A and DS90UB954 for 720p appliction?
For 1080p application,everything works well but for 720p,
input signal is YUV422,PCLK is 74.25M, By querying 954 registers, it is found that the image length and width have changed to 1644*449. It is not clear why the width and length change
954 config:
{0xB3, 0x00}, /* BIST */
{0x4C, 0x01},
{0x58, 0x58}, //for 913
{0x5B, (TI913_ADDR << 1)}, /* TI 913 slave address, it is able to automatically get from T I 913 */
{0x5C, (TI913_ADDR << 1)}, /* TI 913 alias address */
{0x1F, 0x03}, /* 800Mbps csi clock per lane//1.6Gbps csi clock per lane */
{0x32, 0x01},
{0x33, 0x01}, /* 4line /2lane */
{0x20, 0x20},
{0x0F, 0x7F}, /* GPIOs as input */
{0x6E, 0x10}, /* GPIO0->GPIO0, GPIO1->GPIO1 */
{0x6F, 0x32}, /* GPIO2->GPIO2, GPIO3->GPIO3 */
{0x70, 0x1E},
{0x7C, 0xA0}, /* use RAW10 upper 8 bit*/