This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

[FAQ] definition of signal conditioner(redriver/repeater/retimer..)

Expert 4255 points

Replies: 1

Views: 670

Dear experts,

I want to understand the signal conditioner definition. would you explain what is difference between redriver and repeater and retimer ?

Thanks,

JH.

  • JH

    A repeater can be either a re-driver or a re-timer. Please see this e2e post for the difference between the re-driver and the re-timer.

    https://e2e.ti.com/blogs_/b/analogwire/archive/2017/05/01/how-to-select-a-redriver-or-retimer-for-hdmi-2-0-jitter-cleansing

    • A redriver performs signal conditioning through equalization, providing compensation for input channel loss from deterministic jitter such as inter-symbol interference.
    • A retimer is a mixed-signal device that includes equalization functions plus a clock data recovery (CDR) function to compensate both deterministic and random jitter, and in turn transmit a clean signal downstream.

    Re-driver can further be divided into linear and limited re-driver. The difference between linear and limited re-driver is that limited re-driver provides its own TX block which may include swing and pre-emphasis control while linear does not provide TX block, the swing and pre-emphasis comes from the source.

    Thanks

    David

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.