Other Parts Discussed in Thread: SN65DSI84
Dear,
We would like to use STM32F769NI MCU with the following caracterictics :
– LCD-TFT controller supporting up to XGA resolution – MIPI® DSI host controller supporting up to 720p 30 Hz resolution
to AUO TFT Screen C123HAN02.1 which is 2 port LVDS 1920 x 720 (Datasheet can be send on request)
So my simple question is to know if SN65DSI84 can be easily used to interface the STM32F769 DSI output to this 2 ports LVDS TFT ?
Best Regards
David