The on-board Ethernet debugging has the following problems: the network card can be identified, but the PING is different and the network cannot be connected,Test data and SCH see attachment.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The on-board Ethernet debugging has the following problems: the network card can be identified, but the PING is different and the network cannot be connected,Test data and SCH see attachment.
HI :
1,The device itself PING can PING the same.
2,The device PING PC, won't work on PING.
Hi,
I am not able to follow. Please explain your setup, and test steps you are performing and failure you are observing.
Regards,
Geet
1 the device and the computer are on the same network at 169.254.4.1 169.254.4.2, respectively.
2 Settings and computers are connected to the same router, and ping is different.
3 The equipment address is 169.254.4.1. Ping this address on the device side.
4 How do I read the value of 0x0001? In what circumstances is it read? What is the value of reading? Please provide a detailed description?
Hi,
Please refer to User Guide of the EVM for details on MDC and MDIO Pin. You can use USB-MDIO Tool to connect to MDC/MDIO pin to read the register of PHY.
http://www.ti.com/tool/USB-2-MDIO
Regards,
Geet