Hi team,
Does TCA9548A have any issue under below operating voltage?
Thanks!
Best,
Jason
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jason,
It would be better to operate at a lower VCC level. At VCC = 3.3 V, the "Vpass" voltage would be about 2 V (see Figure 14 in the datasheet). This means that any voltages lower than 2 V would be passed through the device. The master side's high level of 1.65 V is below this, and so the downstream channels would also have a high level of close to 1.65 V rather than the desired 5 V level.
Regards,
Max