Other Parts Discussed in Thread: AM3358, TLK105
I use DP83822 in design with AM3358 as PRU PHY.
In Datasheet page 8 is : During RESET: RX_CLK on pin 25 is output O with PD.
It means Output active LOW?
After the power up, this line is used to configure our Sitara.(LCD data 14) Therefore his circuitry did not work, because our device drives this pin to ground.
Is there any recommendation, how to overcome this behavior?
"After power up the system, our device pulls the pin 25 RX_CLK to low, even if my customer adds a 1kOhm pull up resistor to the line.
This is completely different to the behavior from our TLK105."
Best regards,
Jiri