Other Parts Discussed in Thread: LMH0397
Does the device require any special setup when being used for rates other than SMPTE? We are trying to use it at the 4x FibreChannel rate of 4.25Gbps, which doesn't match any of the reclocker rates.
Sometimes the device requires several resets (performed by power-cycling the board) before an error-free output is observed. Additionally, performance improves when the board has been running for a few minutes. We're not sure if setup or signal integrity is the greater factor.
Thanks!