This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

DS90UB954-Q1: DS90UB954 part with DS90UB913A issue

Intellectual 930 points

Replies: 1

Views: 72

Part Number: DS90UB954-Q1

Dear 

what is the different of 913 and 953  to part with DS90UB954 ?  if there any demo code ? or register set list ,many thanks ~

  • Hi Andrew,

    The DS90UB953-Q1 is for interfacing with CSI Imagers versus the DS90UB913-Q1 which requires imagers with a parallel output. The DS90UB954-Q1 can interface with both of these, however it's default mode is set-up to interface with the DS90UB953-Q1. If you are using the DS90UB913-Q1 then you'll need to set-up the DS90UB954-Q1 for RAW mode for backwards compatibility (see 7.4.2 and Table 2 of the DS90UB954-Q1 Datasheet). Also, if using the 913, then set the back channel to 2.5Mbps in register 0x58[2:0]

    Regards,

    Mandeep Singh

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.