This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

DP83TC811S-Q1: questions about DP83TC811

Genius 4980 points

Replies: 1

Views: 103

Part Number: DP83TC811S-Q1

Dear TI Experts,

 We are using DP83TC811S, the CPU is NXP I.MAX 8,using the RGMII protocal

And from the I,MAX8 datasheet,it‘s said that  ENET0 support RGMII at 1.8V only~

But from DP83TC811S datasheet, the VDDA voltage is 3.3V; Is it OK to work together?

I'd like to know is their anything need to pay attention to when I design it?

Best Regards

  • Hi Qianqian,

    You can use the DP83TC811S-Q1 with the IMAX8.

    Please configure VDDIO for 1.8V operation. VDDA is for the PHY core supply.

    VDDIO is for the IOs.

    Best regards,

    Ross Pimentel

    Ethernet - Applications Engineer

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.