Other Parts Discussed in Thread: TCA9535
I assume the initial value of interrupt pin is High-Z due to open-drain.
However I found it keeps low during power off to power on.
I didn't connect anything to I/O and I2C on PCA9535.
Just have below circuit.
- 3.3V on VCC
- grounding on GND
- use 10K ohm to pull-up interrupt pin
My question:
- Is it correct that "the initial value of interrupt pin keeps low during power off to power on" ?
- If so, How can I modify the initial value of interrupt pin to HIGH-Z ?