Tool/software: Code Composer Studio
in e2e.ti.com/.../808402,Junqiang Shi reply :
1. 941/948 is one bridge to transmit the input video signals from DSI port to OpenLDI output. In 948 side, it has no video timing re-gen., in 941as side, dependent on the input DSI timing mode from SoC, 941as can re-gen. input video timing. if SoC output is sync. pulse mode, 941as can recover it well, for sync. event mode, 941as can generate the video input timing with reg. setting. pls check DSI indirect reg. 0x20 in 941as d/s.
i read newest 941 datasheet ,there are only DSI_HSW_CFG and DSI_VSW_CFG Regs for setting,how to set hbp,hfp,vbp.vfp?