Hi Team,
My customer has a camera module which uses a '913 Serializer taking parallel pixel data. On the other end, there's an ECU which has a 954 that produces CSI MIPI to and FPGA w/ MIPI input. We have a couple questions on the RAW modes- our understanding is we need to set 954 into RAW mode when used with 913.
Question(s):
1) Please confirm transferring YUV422 8b parallel data through 913 SER across FPDLink and Deserialized by 954 DES is feasible?
2) If so, what is the CSI Data Type (DT_ that we would expect to see at the output of the 954 Deserializer? DT = h E (YUV422) or DT =h A (RAW8)
3) What is the line rate calculation if 8 bits of data + 2 sync bits. Assume fPCLK ~ 60MHz. If the equation can be provided, that would be best. 4 lane MIPI PHY is the interface from the deserializer to our FPGA.
Thanks,
Mitchell