Hi,
In using DP83848I ,I noticed this doc http://www.ti.com/lit/an/snla088a/snla088a.pdf
I'm not sure these two transformers can replace each other?Please let me know what is the difference in use,thank you very much!
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
In using DP83848I ,I noticed this doc http://www.ti.com/lit/an/snla088a/snla088a.pdf
I'm not sure these two transformers can replace each other?Please let me know what is the difference in use,thank you very much!
Thanks!
Hi Peng,
One schematics shows discrete transformer, where transformer is separate from RJ-45 connector. The other example is of a RJ-45 with transformer integrated inside. Both examples are acceptable as long as the electrical specifications are satisfied. Because their construction is very different, they will not be footprint compatible. DP83848I can work with both discrete transformers and integrated transformers.
-Regards
Aniruddha
Hi Peng,
The dots are used to convey the polarity of the coupling between the primary and secondary winding of the transformers. For this purpose, the winding will not affect the transformer performance. If the footprint and the electrical parameters are matching then the two transformers can be used. It is important to make sure that magnetics meet the requirements in the datasheet of the PHY.
-Regards
Aniruddha