Please refer to Fig.1 ~ Fig3.
Fig.1 shows that it is accessed 100.5ms after reset release.
Fig.2 shows that the TD_P-TD_M signal is not output even if the TX_D0 signal is output when accessed 100.5ms after reset release. (In case of abnormality)
Fig.3 indicates that the TD_P-TD_M signal is output when the TX_D0 signal is output when accessed 10 seconds after reset release. (Normal)
Why is the TD_P-TD_M signal not output even though the TX_D0 signal is output when accessed 100.5ms after reset release?
The bootstrap settings are as follows.
Only COL is set to MODE3 (set to 100BASE-FX)
Set other defaults
24 # pin is not connected.