Hi,
My final goal is to change the (source) PDO bank based on the Barrel Jack Detect Event.
In testing if this would work, I have set the 'Active PDO Bank Follows EP' bit. I then tried setting Externally Powered in Port Control, but to no effect. It doesn't matter if it is turned on or turned off, it always advertises the PDO bank set as 'Active PDO Bank'.
Furthermore, changing the PDOs in bank 0 to 'Advertise Only If Externally Powered' and setting 'Active PDO Bank' to bank 0, I again tried switching between EP and not EP in Port Control, but still no effect. It will only advertise PDO 1, which is always advertised.
I'm using GUI Build Version 6.1.1.
Great thanks for your help.
Matthijs