hi i am facing problem with installation of this driver
my driver look like below;
tcan4x5x: tcan4x5x@0 {
compatible = "ti,tcan4x5x";
reg = <0x0000 0xFFFF>;
#address-cells = <1>;
#size-cells = <1>;
spi-max-frequency = <18000000>;
bosch,mram-cfg = <0x0 0 0 32 0 0 1 1>;
data-ready-gpios = <&gpio1 14 GPIO_ACTIVE_LOW>;
device-state-gpios = <&gpio3 21 GPIO_ACTIVE_HIGH>;
device-wake-gpios = <&gpio1 15 GPIO_ACTIVE_HIGH>;
reset-gpios = <&gpio1 27 GPIO_ACTIVE_LOW>;
};
m_can1: can@20e8000 {
compatible = "Bosch,m_can";
reg = <0x020e8000 0x4000>, <0x02298000 0x4000>;
reg-names = "m_can", "message_ram";
interrupts = <0 114 0x04>,
<0 114 0x04>;
interrupt-names = "int0", "int1";
clocks = <&clks IMX6SX_CLK_CANFD>,
<&clks IMX6SX_CLK_CANFD>;
clock-names = "hclk", "cclk";
bosch,mram-cfg = <0x0 0 0 32 0 0 1 1>;
};
what is the problem in the driver ?how i correct it?