This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65DP141: DP141 eval board showing bad results with DP cables

Part Number: SN65DP141
Other Parts Discussed in Thread: TDP142

 

Customer request for DP 6ft @12Gbps. Found It's 141 solution and purchased DP141RLG Eval module.

Upon receiving the DP141 module we ran some basic DP cable tests with the device. The goal is to move 12Gbps over a 6 foot DP cable. However when using as little as 2ft its output was pathetic .In fact the cable by it self  was just a little bit worse.

We must be doing something majorly wrong or the part cannot support DP over any longer cable length. At 12Gbps there is almost no eye at all.

The 4 wave form images show this with DP at 28AWG twin-ax.

As for Eval set up

Alll jumpers were set for:

Max EQ Settings                   Hi Hi

I2C mode                               Low

Cable/trace mode to Cable    Hi

Gain set for high                    Hi

After these initial set ups we then changed them to many other configurations with the same or worse results.

Can you explain why this is happening? Is the part N/A to DP cable? The data sheet seems to claim this and the Eval comes equipped with DP connectors.

I  have attached the Eye Patters to demonstrate what we measured. We sincerely hope we can achieve this with TI. The customer is very big and would love to use a domestic firm like TI.

Thank You

Jeffrey Boccaccio

InVisions Technology