Currently I am working on project in which I have used this part number to generate one differential signal. As per datasheet the change in the output differential voltage is -400mV to +400mV. But during testing I have found out the differential swing is from +3.6V to -3.6V. I checked the reference board also and I found the total differential swing of around 6.5V. Any suggestion?