Other Parts Discussed in Thread: TVS2200,
HI there, I have a customer that has some questions. Schematic related questions I will send internally.
1) what package resistor should they use for the components Cap and 3.48 ohm shown for the snubber circuit (Figure 35 in datasheet), 0402 / 0603 / 0805 / 1206 ?
1b) customer is also using a TVS2200 for protection right at the USB-C connector, is this sufficient to prevent protection for any voltage spikes above 20V? I noticed in an e2e post we recommend this part. Have we done any test data for this? Any preference to snubber vs TVS or having both populated?
2) On 3V3_LDO the output is 25mA max, even when fed from an external switcher on 3V3IN that can provide more than 25mA ?
3) PP_CABLE – since we they are not using it, then pin must be grounded or best to have pull up and pull down option for future need?
4) BOOT - ADCIN1 if our equipment is going be the sink device, using a power adaptor of 15V @ 3A max & we will also use it as OTG 5V up to 1A, what is the best option to program for ADCIN1 among the many choices ?
- Dead battery – BP_Wait for 3V#_Internal ?
- Configuration 3 ?
5) Does an errata exist for this device ? The latest firmware revisions are in the TI config tool. Do we have any H/W errata? I believe no but need to ask….
6) There is no indication that the signal MISO (pin 5 on the SPI Flash) needs a pull. Does it need a pull-up ?
6b) There is no indication that the signal CLK (pin 6 on the SPI Flash) needs a pull. Does it need a pull-up ?
Many thanks for your help Guys!