Hi,
This is Zihao, and recently I was handling the issue about the two different port connected to the CPU boards, one is the fibre ethernet which could be found from the PC, however the other one is the ethernet port which failed.
In the last few days, I recorded the graph of MDIO and MDC of these two different board, and found that the data was different in device address, register data, which shown below,
ethernet port: 1 01 10 00000 00001 10 0111 1000 0000 1001 1
fibre port : 1 01 10 00001 00001 10 0111 1000 1100 1101 1
from the data, it seemed that fibre should be in the correct condition, however it is not.
Now I am trying to test the data from other pins for DP83640, which is TX_EN, TXD_0, TXD_1, RXD_1, RXD_0, RX_ER. But unfortunatly, I got nothing from them.
I wonder there would be some methods to communicate with the DP83640, therefore I could record the data from the pins above.
please help me .
Zihao