Other Parts Discussed in Thread: DP83TC811
Hi Team,
My customer is evaluating DP83TC811S-Q1 and has some questions as follows,
Q1. Under power off, VDDA=VDDIO=0V of the DP83TC811S-Q1, if 100BASE-T1 signals are inputted into TRD_P/M of the DP83TC811S-Q1, are there any issues on the DP83TC811S-Q1?
Q2. Datasheet of the DP83TC811S-Q1, Timing Requirement on page 14, has ramp rate of VDDA and VDDIO at Power-Up Timing.
VDDA and VDDIO ramp rate: Min=0.165 V/ms, Max=33 V/ms
If the ramp rate was faster or slower than Min-to-Max range, what would happen on the DP83TC811S-Q1?
Especially, if the ramp rate was faster than Min spec, what would happen on the DP83TC811S-Q1?
Q3. If the DP83TC811S-Q1 is Slave, is it possible to do the Compliance Test?
Thank you.
Best Regards,
Koshi Ninomiya