Other Parts Discussed in Thread: TUSB216, TUSB216EVM
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
For this application I would recommend using TUSB216, our latest USB 2 redriver. Could you tell me the state of CD, ENA_HS, DP and DM when the failure is seen? TUSB211 could be entering compliance mode. This is described in section 5.1 USB 2.0 High Speed Downstream Signal Quality Testing of the TUSB2XX Implementation Guide.
Hi Malik Barton,
Thanks for your reply.
We left the CD and ENA_HS floating, so I can't get the state of them.
Hi,
Your schematic did not post correctly could you try again or send it over direct message? Are you able to probe DM and DP? What connectors are on your adapter board, if any? If is workable I recommend getting TUSB216EVM to evaluate your system and probe CD, ENA_HS, DP and DM.
Hi Malik Barton,
Hi,
Thanks for posting the schematic. I do mean using an oscilloscope to probe DM and DP using high impedance probes, is this possible for you? As an alternative do you have a USB 2 data analyzer that could be used to compare pass and fail case? You could also evaluate the system using the TUSB216EVM if you have a Type-C to A cable. TUSB216EVM would replace the adapter board in your testing.
Hi Malik Barton,
Thanks a lot. It's unconvenient for me to probe DM and DP.
If I use TUSB216EVM, do I need to connect SDA, SCL, RX_SEN / ENA_HS, RSTZ, CDP_ENZ?
Hi,
Using the EVM you do not need to connect SDA, SCL, RX_SEN / ENA_HS, RSTZ, CDP_ENZ to your system. These pins can be controlled external to get the different GPIO settings of tUSB216.