Other Parts Discussed in Thread: TPS65987D, LM34936
Tool/software: Code Composer Studio
Hi,All:
upon the original the charge issue(Dell_5370), it's inrush over the IC spec(max support to 20A,actually current is 24.2A).
according the inrush formual(I=Cload*(DVout/Dt)),i change the PD voltage (from 20.3 to 19.68V)after,it charge normal for the NB in Ambient 25dgree.
but charge 1hour after, maybe the temperature rise on the board,appoximately 40-50dgree .
then pull out the cable from the docking. next re-plug in it to the docking for re-charge.it's fail.
i am check the PPHV's Rds of tps65987D. in the datasheet show 25-33mR at Tj=25 dgree.
doesn't show the resistance of higher Tj of tps65987d.
how many is it on higher temperature?
like this, could you help to me explain the reason?(Ta=25dgree be OK, rise to 50dgree can't charge)
if support the NB, may you with your team add some comment or better solution for it?
you can refer the link "e2e.ti.com/.../874161 for the original issue detail.
thanks!