Other Parts Discussed in Thread: TPS65987, TPS65988DJ
Out of the box, the TPS65988DJEVM functioned with USBC data and Displayport outputs.
Once programmed using the TPS application customization tool, USB data remained functional however Display port has been unable to hot-plug detect when using either usb-c port connections. This results in no display output from the TPS65988DJEVM via the USB-C ports. Re-flashing with the EVM Firmware (Recovery) has not fixed the issue.
Prior to initial programming of the device, I entered debug mode and took note of the settings. I have re-applied these within the application customization tool and re-flashed the EVM board. The issue is still present.
A soft reset does not rectify the issue.
What settings can be preventing displayport from operating after being re-flashed with the recovery firmware?
Is the original firmware on the evaluation module available?