We are using TUSB4041 in our design. It is a 4-port hub with one hub connected to the PC, and three of the downstream ports each connected to one more hub. Each of them are then connected to other USB endpoints.
We are getting some intermittent strange power-up operation. Power cycling looks good: 1.1v before 3.3v, small delay until reset is released.
When power is applied and everything is in a good state (PC is connected and all hubs are operational), if I apply a reset signal to any hub, that hub draws an extra 220 mA from the 1.1v rail. Is this normal operation? I would of course expect the current draw to go down when it is held in reset. I couldn’t find anything in the datasheet referring to reset current. The only note in the current-draw table is that the current shown was “after reset”.