Hi
Let me have a question about TL16C2552.
My customer wants to know whether is there any problem on operation, if a clock with the jitter inputs to TL16C2552,
The details are as follows.
We are currently studying clock supply to the TL16C2552 using the following route.
Oscillator ⇒ FPGA (internal PLL) ⇒ TL16C2552
From the jitter performance of the output terminal of the FPGA, the clock frequency input to the TL16C2552 is
targeting to 3.072MHz and it is expected to be 2.96MHz (min), 3.071672MHz (typ), 3.191348MHz (max).
We are going to use TL16C2552 at a baud rate of 9600bps. (So internal 20 division)
After checking the data sheet, there was no description about the specifications for the input clock (accuracy, frequency width, Duty, etc.)
So could you tell me whether is there any problem on operation, if a clock with the jitter inputs to TL16C2552?
Regards,
Jo