Dear support team;
I would like to connect DS90UB962 and 3 x DS90UB953.
Camera specification is 60fps ans 2Mpix.
3 cameras are same modules.
I am worried about bandwidth.
Could you tell me the feasibility of this system?
B.R.
Sugiyama
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear support team;
I would like to connect DS90UB962 and 3 x DS90UB953.
Camera specification is 60fps ans 2Mpix.
3 cameras are same modules.
I am worried about bandwidth.
Could you tell me the feasibility of this system?
B.R.
Sugiyama
Dear Hamzeh-san;
Thank you for your quick reply.
I will confirm the data type to customer.
Please wait for my information.
Thank you for your patient.
B.R.
Sugiyama
Dear Hamzeh-san;
I got the data type information.
The data type is RAW12.
Could you confirm this combination?
If not transfer, reduce the image size (frame rate is 60fps).
In this case, could you tell me the image size that can be transferred?
B.R
Sugiyama
Hello Sugiyama-san,
calculating the CSI-2 Throughput of the Sensor = 2Mp x 60Fps x 12 bits x 1.25 blanking = ~1.8Gbps.
Using 3x Cameras make = 1.8Gbps x 3 = ~5.4Gbps.
One 962 can support up to 6.4Gbps of CSI-2 data, which means you can use 3x Cameras with one 962 without any limitations.
BR,
Hamzeh
Dear Hamzeh-san;
Thank you for your great support.
I understood the calculation method.
Thank you very much !
B.R
Sugiyama