This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN65HVD01: updated part to replace XR33202

Part Number: SN65HVD01
Other Parts Discussed in Thread: THVD1450

Hi,

Do we have upgraded part of SN65HVD01 supporting both 3.3V and 5V RS-485 to replace XR33202? Thanks.

Best Regards.

Chen

  • Hi Chen,

    We saw your email on this topic earlier and responded to it, so we can keep the discussion there.  For the benefit of the forum, I would suggest THVD1450 as a general recommendation for RS-485 transceivers supporting both VCC = 3.3 V and 5 V.

    Max