This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB954-Q1: Paired with UB933(YUV422-8bit input)

Part Number: DS90UB954-Q1

Hi team,

We have questions about UB954 and UB933 cooperation for encoding and decoding.

DS90UB933: Input format:YUV422-8Bit

                      Operating mode:10-bit Mode,but only use DIN[7:0]

In this configuration of UB933, we configure the UB954 register 0x70 = 0x1E(Only one input),register 0x7C = 0xC1.

Can this configuration decode the signal transmitted from 933 correctly.Now that our configuration has abnormal colors on the display side, we suspect that U or V signal is missing two of them

Best regards,

Alec Li