Hi,
My question is that :i am Making a project on Laser distance measure using time of flight technique
Now Iam using ONET4211LD Laser driver for laser diode
and for the receiving side first Transimpedance ONET2591TA and then Limiting amplifier ONET1191P by using this i want a pulse output (max:2V output)so that i can make stop pulse for my time calculating chip will it be possible by using this only i can make a pulse output and use it as a stop pulse(Minimum pulse duration is 2.5ns)
please give me on this issue.....
.........Tushar Patel............
Patel,
The TIA and PA can detected a 400MHz pulse but the max output voltage from the 1191P is only 700mVpp differential. I do not know if this is sufficient for you.
Alex.