Hi,
currently I'm evaluating limiting amplifiers for 10G optical communications. So I found the limiting amplifier ONET1191P. After reading the data sheet, I've got some questions.
- The frequency response in Fig. 3 shows a peak at ~5GHz. What is the reason for this peak? Is it maybe to compensate of the lowpass behavior of a preceding TIA?
- The differential input return gain shows a dip at ~4GHz. What is the reason for that?
- Does the LOS assert/deassert voltage in figure 10 refers to the input voltage or the output voltage? If it refers to the input voltage, why is it not possible to put the LOS threshold to a meaningful value such as 10 mVpp (the input voltage where the outputs are typically limited)?
Thanks,
Raphael