I am looking at the ONET1141L as a driver for my DML device. I see that it uses the I2C bus to configure the device.
Question 1, Can more than one ONET1141L be used on the same bus? I see in the documentation where it talks about the address of the device. Is this hard coded or can I set different devices to different addresses?
Question 2, If the answer to '1' is hard coded, can I still tie all of the devices on the bus if I want the same information to be passed to all of the devices? I am new to using I2C. I was not sure if there is an acknowlege sent back by the slave when data is transferred.
Any help with this will be greatly appreciated.
Thank you,
Mike Nycz