Hello.
Is rx clock produced even when receiving signal is lost ?
If signal is lost, RXD[15..0], RX_DV and RX_ER should be high; but I don't know whether RX_CLK is produced or not.
Thank you...
Petr
Petr,
In the case where the serial input to the device (TLK2501/TLK1501..) is lost, the RX_CLK will likely track the device's GTX_CLK or the CDR as it tries to lock. You can check this by removing the GTX_CLK and observing the behavior of the RX_CLK.
Thanks,
Atul Patel
Texas Instruments
Mr. Patel,
I will try to ask by another way. Can I clock receive data bus terminals (signals RXD, RX_DV and RX_ER) by RX_CLK when input serial signal is lost ? I purpose to use it for the detection of loss of signal.
Petr Burian.
When the incoming serial signal is lost, the parallel output data singles (RD) are not valid and RX_CLK is not guaranteed to be at the correct frequency needed for your application so using RX_CLK may not provide expected results consistently. The RX_DV/LOS pin provides LOS condition indication for the device.
Atul