Hello I am using the DS92LX1622 /21 in Camera mode. I have an SC18IS600 I²C Master and can communicate with the Deserializer connected direct to the I²C master.
The M/S Pin at the Deserializer is high, so the Deserializer is in slave mode. Now I want to programm the Serializer, connected to drilled two wire kabel. I set the adress of serializer in deserializer (Adr 7). But the Serializer is not responding. In wich mode the serializer has to be? Master / Slave ? I tried both, but nothing happens.
I can´t find the failure, wich addresses do I have to set? Can anyone help me? Did anyone have a sample code how it works?
Thanks in advance,
Sebastian Miesner