• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Interface » High Speed Interface » High Speed Interface Forum » LMH0307 termination
Share
High Speed Interface
  • Forum
  • Files
  • E2E Wiki
Options
  • Subscribe via RSS
Check out
Analog Wire blog
  • $core_v2_blog.Current.Name

    RS-485 - Who says you can't teach an old dog new tricks?

    Posted 4 days ago
    by Neel Seshan
    Would you agree that RS-485 has turned out to be one of the most...
  • $core_v2_blog.Current.Name

    Filter for thought

    Posted 5 days ago
    by Soufiane Bendaoud
    Have you ever wondered how engineers designed active filters...
  • $core_v2_blog.Current.Name

    Let’s take this driver out for a spin

    Posted 11 days ago
    by Soufiane Bendaoud
    Before I suggest a suitable op amp to drive an ADC, I look at...

LMH0307 termination

LMH0307 termination

This question is not answered
Aaron Spaete
Posted by Aaron Spaete
on Aug 06 2012 10:24 AM
Intellectual1045 points

Team,

My customer has the following question:

Regarding termination of the LMH0307, the datasheet discusses 75 ohm output pull-ups with a 750 ohm RREF resistor. I installed 50 ohm pull-ups to provide a 100 ohm differential output. It looks like the RREF resistor needs to change to 500 ohms as well otherwise I don't get the specified output voltage levels. The datasheet is adamant  it should be 750 ohms, however it only addresses 75 ohm terminations. Am I correct the RREF resistor needs to be 10 times the single ended termination resistor value to generate the correct output voltage level?

Regards,

Aaron

Report Abuse
  • Reply
You have posted to a forum that requires a moderator to approve posts before they are publicly available.
All Replies
  • Gary Melchior
    Posted by Gary Melchior
    on Aug 06 2012 14:51 PM
    Intellectual1390 points

    Please provide more details about this application.  What specific output amplitude is required from the LMH0307, and is this single ended or differential?  And what is at the receiving end of the cable?

    Typically, there is an SDI adaptive cable equalizer (such as the LMH0344, LMH0384, or LMH0394) at the other end of the cable to receive the signal.  For coaxial cable, the single-ended amplitude of the signal going into the cable should be 800 mVP-P in order for the equalizer to properly equalize the signal.  For differential cable, the equalizer would be configured to receive a differential signal, and in this case the amplitude of the signal going into the cable should be 800 mVP-P differential (so it would only be 400 mVP-P single ended).

    Using 75 ohm pullup resistors, the LMH0307 will drive 800 mVP-P single ended into 75 ohm coaxial cable.  With 50 ohm pullup resistors and RREF at the default value of 750 ohms, the single-ended output voltage is about 533 mVP-P ((50/75) * 800).  (The differential output voltage is about 1066 mVP-P.)  Due to current limitations, the LMH0307 is not able to drive 800 mVP-P single ended into 50 ohm loads.  The RREF resistor value can be decreased in order to increase the output amplitude, but the lowest value of RREF that should be used is 665 ohms which provides a single-ended amplitude of about 600 mVP-P into a 50 ohm load.

    However, if the intent is to drive a signal into the cable so it can be received differentially by an SDI cable equalizer at the other end, then I would recommend to use the 50 ohm pullup resistors and set RREF to 953 ohms, which will provide 800 mVP-P differential (400 mVP-P single ended) into the 100 ohm differential cable.

    SDI
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Joseph Stramaglia99021
    Posted by Joseph Stramaglia99021
    on Aug 06 2012 15:46 PM
    Prodigy115 points

    Gary,

     

    Thanks for the information! This is a similar design to the one shown in this forum post (although not identical) http://e2e.ti.com/support/interface/high_speed_interface/f/138/p/199016/716411.aspx#716411

     

    So the output (setup as a 100ohm differential output) from the LMH0307 will be AC coupled to a lightning protection transformer (I've already given them National's paper on lightning protection using other things) through a custom cable, to another transformer and then to the an LMH0344. 

    It was important to know just how low the Rref could safely be (the older comlinear parts used to give you a reference chart / graph of possible Rref values). I know this is off-dataasheet, but they have been using these for years for various interfaces like this.

    Any other recommendations you'd like to offer would be appreciated, although we had a recent conference call with the High Speed Interface guys and the LMH0307 / LMH0344 reference was what they settled on too.

    Joe

     

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Gary Melchior
    Posted by Gary Melchior
    on Aug 06 2012 19:27 PM
    Intellectual1390 points

    I would recommend using an RREF resistor of 953 ohms for this application.  With 50 ohm output pullup resistors, the LMH0307 will drive an 800 mVP-P differential signal into the cable.  Assuming there are no other losses in the data path (besides the cable), this is the ideal launch amplitude to allow for the best equalization performance of the LMH0344 equalizer on the other end of the cable.

    They should not attempt to drive an 800 mVP-P single-ended (1600 mVP-P differential) signal into the 100 ohm differential cable, for the following reasons:

    1. This exceeds the current limitations of the LMH0307.
    2. The LMH0344 equalizer expects an 800 mVP-P signal going into the cable.  The LMH0344, configured differentially, would receive this 1600 mVP-P signal, assume the cable is much shorter than it actually is, and proceed to grossly under-equalize the signal, increasing jitter and shortening the cable reach.
    SDI
    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use