The DS90UB913/914 datasheet recommends using an external oscillator as its reference clock and then goes on to note that the pixel clock must be a specific ratio to the external oscillator in the 10-bit and 12-bit high frequency modes. There is no mention of a required ratio for 12-bit low frequency mode but I suspect it is 1:1. Is this true?
Unless I misunderstand the datasheet, these fixed ratios mean it is impossible to change imager settings (or change imagers) if it would result in a different pixel clock rate unless I also replace the oscillator. This makes me want to use the pixel clock as the reference. How common are jitter issues using this mode? My serial link is less than a meter long but needs to be as thin as possible - possibly 30AWG 100 ohm twin-ax.
Thanks,
-Carl