Hi,
I use the DS90UB925 / DS90UB926.
The transmit datas are 18Bit, I2C, I2S, and five IO's.
The I2C I do need for the touch communication, but I couldn't found a clear answer about the speed.
The confusing item is the down stream datarate from 926 to 925. On the datasheet page 10 is written a speed of >50kbps and on page 16 is a speed of 10Mbps; Is it possible to have a downspeed datarate of 400kbps on the I2C?
Next Question is quite similar: Is it possible to have a down stream datarate of 500kpbs on a GBIO ?
Thank youn very much for a fast answer.
Best regards
Thomas Feller