Hi,
Is it possible to have multiple Desirializers for one Serializer or a way of repeating the information to multiple locations.
Thanks
Danny
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Is it possible to have multiple Desirializers for one Serializer or a way of repeating the information to multiple locations.
Thanks
Danny
Danny,
I have contacted the apps engineer responsible for these devices and they will take a look at your question. Thanks.
Hi Danny,
I have pulled the figures below from the DS90UB928Q datasheet. The DS90Ux925/6 and DS90Ux927/8 can be placed in repeater mode for a maximum of 9 displays.
1. Video Data – Connect all FPD-Link data and clock pairs
2. I2C – Connect SCL and SDA signals. Both signals should be pulled up to VDD33 or VDDIO = 3.0V to 3.6V with 4.7kΩ resistors.
3. Audio (optional) – Connect I2S_CLK, I2S_WC, and I2S_Dx signals.
4. IDx pin – Each Transmitter and Receiver must have an unique I2C address.
5. REPEAT & MODE_SEL pins — All Transmitters and Receivers must be set into Repeater Mode.
6. Interrupt pin – Connect DS90UB928Q-Q1 INTB_IN pin to the DS90UB927Q-Q1 INTB pin. The signal must be pulled up to VDDIO with a 10kΩ resistor.
Regards,
Mike