Posted on behalf of another users:
Regarding the Typical Application Diagram for the DS100BR210, are AC coupling capacitors needed on both sides of the DS100BR210 device?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Posted on behalf of another users:
Regarding the Typical Application Diagram for the DS100BR210, are AC coupling capacitors needed on both sides of the DS100BR210 device?
The DS100BR210 does require AC coupling capacitors on both the input and the output. With regards to the Typical Application Diagram in the DS100BR210 datasheet, however, there is one set of AC coupling capacitors in between the two devices which are redundant and can be removed. Only one set of AC coupling capacitors is required between the two devices.